Library Waveform (Carrier n)

The N7624C Signal Studio Pro for LTE/LTE-Advanced FDD 2027 software enables you to import waveforms to evaluate multi-standard radio (MSR) effects on LTE/LTE-Advanced FDD signals.

Below is a list of the Signal Studio waveforms that can be imported into the MSR feature for LTE/LTE-Advanced FDD signals.

  1. Supports high-resolution waveform export, providing better signal quality in the resulting MSR waveform.

  2. Supports high-resolution waveform import and export, providing better signal quality in the resulting MSR waveform.

You cannot recursively import waveforms. That is, an MSR waveform cannot be used as a component waveform in a new MSR waveform. In this case, an error message appears in the status area.

In the figure below, an Library Waveform is selected for configuration. Refer to MSR: Generating a Library Waveform.

Carrier n -- Library Waveform

1. General

2. Baseband

MSR: Generating a Library Waveform

MSR: Using the Waveform Library Manager

Overcoming Test Challenges of MSR Base Station Components and Transmitters